Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Which compilers have two kinds of license (Standard and Professional editions)?

Last Updated:05/17/2017

Question:

Which compilers have two kinds of license (Standard and Professional editions)?

Answer:

The following compilers have two types of license.

  • RL78 Family C Compiler Package (CC-RL), from V1.01.00
  • RX Family C/C++ Compiler Package (CC-RX), from V2.04.01
  • RH850 Family C Compiler Package (CC-RH), from V1.03.00
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family