Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Symbol generation for the stack area and the overlay function (CC-RL)

Last Updated:05/10/2017

Question:

I am using RL78 Compiler CC-RL.

When the -device option is specified in the linker, continuous unused area in the RAM area is sought and __STACK_ADDR_START and __STACK_ADDR_END are generated. At this time, are sections with the overlay specification considered?

Answer:

CC-RL allocates the stack area in consideration of sections with the overlay specification.

For the actual address where sections and the stack area are allocated, refer to the link map file.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?