Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Support for floating licenses for previous versions or revisions of compilers

Last Updated:05/19/2017

Question:

Do you plan to support floating licenses to previous versions or revisions of compilers for which floating licenses are not currently supported?

Answer:

No, we do not plan to support such compilers in that way.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family