Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Message W0523077 (CC-RL)

Last Updated:05/10/2017

Question:

I am using the CC-RL compiler for RL78 devices. I am getting the warning code W0523077. How can I avoid this?

W0523077: Called function should have prototype. 


[ Example ]
void func()
{
;
}
/*Calling from within the function*/
func();

Answer:

Specify void as the argument of the function before its definition.

[ Example ]
void func(void)
{
;
}

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?