Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Guidelines regarding the quantity of floating licenses to purchase?

Last Updated:05/17/2017

Question:

Do you have any guidelines regarding the quantity of floating licenses to purchase?

Answer:

We have no guidelines on that point. You need to consider the number of developers and the scale of the system you are developing when deciding on the number of licenses to purchase.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • Was this article helpful?