Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

E0562011 Message for -DEBUG MONITOR Option_CC-RL

Last Updated:02/07/2018

Question:

I am using RL78 compiler CC-RL and got the following error. How do I resolve this?

E0562011:Invalid parameter specified in option "debug_monitor" : "3E00-3DFF"

Answer:

The error occurs because the end address (3DFF) is smaller than the start address (3E00) in the OCD monitor area specified with the -DEBUG_MONITOR option of the linker. 
Specify the address of the monitor area according to the type of MCU you are using.

Suitable Products

e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?