Skip to main content
Renesas Electronics Europe - Knowledgebase

Data filling for empty spaces (CC-RL)

Last Updated:05/10/2017


I am using RL78 Compiler CC-RL. How can I fill empty spaces with data?


To fill empty spaces with data, you need to specify the range to fill.

In the settings of the linker, specify the output range by the -Output option and the value to be packed by the -Space option.

Note that if you use an IDE, the preceding output range should be specified by the division output file.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family