Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Will there be any area to change other than the internal ROM/RAM areas?

Latest Updated:02/14/2006

Question:

Regarding any of M16C/60 Series with the internal ROM area of more than 192K bytes and the internal RAM area of more than 15K bytes, if the PM13 bit of the PM1 register is set to "0", will there be any area to change other than the internal ROM/RAM areas?

Answer:

If the PM13 bit is set to "0" regarding M16C/60 Series, the internal RAM area will have addresses from 0400h to 3FFFh; the internal ROM area will have addresses from D0000h to FFFFFh. The area to change other than the internal ROM/RAM areas will be from addresses 30000h to CFFFFh for CS0 area and addresses 04000h to 07FFFh for CS3 area.
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN