Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Why can't I download firmware to the USB Monitor Board in 3V operations?

Latest Updated:02/14/2006

Question:

I can't seem to download the firmware to the USB Monitor Board in 3V operations. What's the problem?

Answer:

The firmware must be downloaded during 5V operations. To download the firmware, first select the USB bus-powered supply (5V), and then begin the download.

Note to customers who use M16C/10 Group MCU
 The content above is applicable only to Normal version, but not to T and V versions which operate only at 5V.

Suitable Products
R8C/10
R8C/11
R8C/12
R8C/13
M32C/87
M32C/86
M32C/85
M32C/84
M32C/83
M16C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M30245
M16C/29
M16C/28
M16C/26A
M16C/26