Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Which package of EIAJ, JEDEC, etc. is used for uPD789316GK-XXX-9ET ?

Latest Updated:12/01/2011

Question:

Which package of the following three types is used for the uPD789316GK-XXX-9ET ?

(1) EIAJ type
(2) JEDEC type
(3) Other

Answer:

(2) JEDEC type
Suitable Products
UPD78931x