Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

When will the value of H8S/2345 16bit transferred to general register?

Latest Updated:03/26/2009

Question:

When is the value of the buffer register on the H8S/2345 16bit Timer transferred to the general register ?

Answer:

The value of the buffer register is transferred to the general register on a condition such as compare-match. Setting a value to the buffer register when the timer is stopped does not transfer the buffer to the general register at that time, it will occur at the next compare-match.
Suitable Products
H8S Family