Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

When a clock divided by f(XIN) which is used as the timer count source?

Latest Updated:03/01/2005

Question:

(Clock)  When a clock divided by f(XIN) is selected as the timer count source and the on-chip oscillator is selected in the clock frequency dividing ratio selection bit of the CPU mode register, which is used as the timer count source? [2005/03/01]

Answer:

f(XIN) is replaced by on-chip oscillator output.
For example, if f(XIN)/2 is selected as a count source, it is replaced by Rosc/2.
The same applies to timer 1, A, X, serial I/O, A/D converter and WDT. (#104960)
Suitable Products
7544