Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

When I do not use the NMI pin, can I connect the pin to Vcc directly?

Latest Updated:03/08/2012

Question:

When I do not use the NMI pin, can I connect the pin to Vcc directly? Technical News "TN-M16C-11-9710" states that "The resistor is not necessary when Vcc pin voltage is same or larger than dedicated input pin voltage".

Answer:

The resistor is not necessary, when the NMI pin voltage satisfies the condition described above. But it is difficult to meet the above condition in the system all the time so you should connect the NMI pin to Vcc via the resistor.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A