When '1' is written to the TCWE bit of TCSRWD, is value '1' held until '0'?
Latest Updated:03/26/2009
Question:
When '1' is written to the timer counter W writing enable (TCWE) bit of the timer control /status register (TCSRWD), is the value '1' held until the next '0' is written?
Answer:
Yes, '1' is held until the next '0' is written.
Suitable Products
H8/300H Tiny |
H8/36109 |
H8/36087 |
H8/36077, H8/36079 |
H8/36064 |
H8/36049 |
H8/36037, H8/36057 |
H8/36014, H8/36024 |
H8/3694 |
H8/3687 |
H8/3672 |
H8/3664 |
H8/36912, H8/36902 |