Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What units are used for reprogramming the Flash memory?

Latest Updated:03/01/2005

Question:

(Flash Memory)   The Flash memory is written to in byte units. What units are used for reprogramming? [2005/03/01]

Answer:

The erase unit determines the reprogramming unit for the flash memory, which is in this case is block units. (#104882)
Suitable Products
3803H
3803L
3850A
38D2
38D5