Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What state does the A/D converter go when STP instruction is executed?

Latest Updated:03/01/2005

Question:

(A/D Converter)  What state does the A/D converter go to when the STP instruction is executed? [2005/03/01]

Answer:

The A/D converter goes to stop mode in the state it was in at the time the STP instruction was executed. Therefore, please make sure the A/D conversion has completed before executing the STP instruction.
Even if the MCU goes to stop mode during an A/D conversion, current will continue to flow to the A/D converter. After returning from stop mode, the conversion result will be indeterminate. (#104831)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549