Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What is the difference between "program ROM" and "data flash"?

Latest Updated:01/11/2008

Question:

What is the difference between "program ROM" and "data flash"?

Answer:

Both are flash memory with the same structure. The differences between the program ROM and the data flash are memory size and electrical characteristics (which include the number of rewrites and bus cycles). The bus cycle is one cycle of the CPU clock for program ROM, and two cycles of the CPU clock for data flash.
Refer to the electrical characteristics in the hardware manual for more details.
Suitable Products
R8C/19
R8C/1B
R8C/21
R8C/23
R8C/25
R8C/27
R8C/29
R8C/2B
R8C/2D
R8C/2F
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/33T
R8C/38A
R8C/34E
R8C/34G
R8C/36E
R8C/36G
R8C/38E
R8C/38G
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC