Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What is the A/D conversion rate of this microcomputer?

Latest Updated:02/27/2012

Question:

What is the A/D conversion rate of this microcomputer?

Answer:

Minimum 43 φAD cycles.
* The frequency of φAD must be set as follows:
When VCC1 is 4.0 V to 5.5 V, 2 MHz ≤ φAD ≤ 25 MHz
When VCC1 is 3.2 V to 4.0 V, 2 MHz ≤ φAD ≤ 16 MHz
When VCC1 is 3.0 V to 3.2 V, 2 MHz ≤ φAD ≤ 10 MHz
Example) 1.72 µs when φAD = 25 MHz, 2.69 µs when φAD = 16 MHz, 4.3 µs when φAD = 10 MHz.
However, the max. φAD of the M16C/63 Group is 20 MHz.
Suitable Products
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57
  • Was this article helpful?