Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What is suggested transition for system clock when shifting modes?

Latest Updated:06/09/2005

Question:

(Clock)  What is the recommended transition procedure for the system clock when transitioning between modes ? [2005/06/09]

Answer:

Make sure to transit between modes according to the system clock state transition figure found in the datasheet. (#105200)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549
  • Was this article helpful?