Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What is low input time required when returning from RAM by key-on wake up

Latest Updated:07/04/2003

Question:

(Power Save)   What is the minimum low input time required when returning from RAM backup mode by key-on wakeup?

Answer:

Input for at least one machine cycle to return completely from RAM back-up mode. (#105029)
Suitable Products
4286
4508
4509
4571