Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What is Crosstalk?

Latest Updated:08/01/2005

Question:

What is Crosstalk?

Answer:

This is a phenomenon whereby a change in a signal line propagates on another signal line as noise.
If ringing such as overshoot or undershoot is generated, for example, noise easily propagates, depending on the capacitance between signal lines, and this noise increases under the influence of the inductance of the signal lines.

Suitable Products
 
  • Was this article helpful?