Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What happens when DMA0 and DMA1 are generated at the same time?

Latest Updated:03/15/2012

Question:

What happens when DMA0 and DMA1 are generated at the same time?

Answer:

When DMA0 and DMA1 are generated simultaneously, DMA0 is executed first.
After DMA0 is completed, the CPU uses the bus for one access, and then DMA1 is executed.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A