Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What does "+4KB" mean when "xxKB+4KB" is used for ROM capacity?

Latest Updated:02/27/2012

Question:

What does "+4KB" mean when "xxKB+4KB" is used for ROM capacity in the Flash memory version?

Answer:

It refers to a data area. This data area can be used for placing table data or for writing a value serially, as in EEPROM. It is also possible to place and run programs.
Because +4KB Flash area is located in the near area, high speed memory access is possible.
Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A(M16C/62T)
M16C/62M
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/30P
M16C/29
M16C/28
M16C/26A