Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What causes this non-map error and what is the countermeasure?

Latest Updated:12/01/2011

Question:

A non-map break occurs in the debugger and the program execution stops.
No error in particular occurs in the compiler and linker.
What causes this non-map error and what is the countermeasure?

Answer:

It is not possible to tell based solely on this information.
If a non-map break occurs and program execution stops, that the data used to access problematic non-mapped areas should remain in the trace data.
Please check whether this is really access to memory other than the relevant memory.
Suitable Products
78K Family