Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What causes IIC bus transfer rate master transmit/receive operation?

Latest Updated:03/19/2008

Question:

During master transmit/master receive operations, I can only get a IIC bus transfer rate which is half of the rate which I set. What could be causing this?

Answer:

The pull-up resistance of the board may be so high that the SCL rise time is over the limit for the IIC bus. This would trigger the bit synchronization circuit. Therefore, please revise your pull-up resistance to make SCL rise time, within the MCU's permissible current range, to 1000 ns max for up to 100 kbps, or 300 ns max for up to 400 kbps. In addition, the bit synchronization circuit monitors the SCL pin after it is released from being driven low, to check whether SCL has risen to high level or not. During the monitoring period, IIC is determined by the IICX bit and IIC2 by the CKS3 and CKS2 bits, according to the transfer rate which was set. If the SCL pin cannot be confirmed to be high level during this monitoring, the bit synchronization circuit judges this as SCL having not yet risen to high level, and essentially skips one SCL fall time. As a result, output becomes half (high:low = 3:1) of the transfer rate which was set.
Suitable Products
H8S/2643
H8S/2630, 2639, 2638, 2636, 2635
H8S/2633
H8S/2556, 2552, 2506
H8S/2472, 2463, 2462
H8S/2378, 2378R
H8S/2368
H8S/2268, 2264
H8S/2258, 2239, 2238, 2237, 2227
H8S/2199R
H8S/2189R
H8S/2168
H8S/2148, 2144
H8S/2140B
H8S/2138, 2134
H8S/2128, 2124
H8S/2117, 2117R
H8S/2116
H8S/2114R
H8S/2111B
H8S/2110B
H8SX/1668R, H8SX/1668M
H8SX/1663
H8SX/1658R, H8SX/1658M
H8SX/1653
H8SX/1648G, H8SX/1648H
H8SX/1648A, H8SX/1648L
H8SX/1638, H8SX/1638L
H8SX/1622
H8SX/1544