Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What's the status of P110-P115 to PWM outputs of TOM and TOU?

Latest Updated:12/26/2005

Question:

Regarding the PWM output disable function of the TOM timer and the TOU timer, I would like to know what status the ports (P110-P115) corresponding to PWM outputs of TOM timer and TOU timer will assume when PWM output is disabled.

Answer:

The ports (P110-P115) in relation to TOM timer and TOU timer always go to a high-impedance state no matter which mode they are in.
Suitable Products
32172, 32173
32180
32185
32186
32192
32195
32196