Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Ports P20-P27 to input mode; key-on wakeup on for input P20

Latest Updated:03/01/2005

Question:

(Interrupts)   Can ports P20 to P27 be set to input mode and key-on wakeup enabled only for input to P20? [2005/03/01]

Answer:

No.
Setting ports P20 to P27 to input mode enables key-on wakeup. (#104952)
Suitable Products
3823