Meaning of high input current IIH and low input current IIL
Latest Updated:10/05/2016
Question:
What is the meaning of IIH (high input current) and IIL (low input current) shown under electrical characteristics?
Answer:
IIH (high input current) is the leak current when a high level is input to the input pin.
IIL (low input current) is the leak current when a low level is input to the input pin.
IIL (low input current) is the leak current when a low level is input to the input pin.
Suitable Products
R8C/32C |
R8C/33C |
R8C/34C |
R8C/35C |
R8C/36C |
R8C/38C |
R8C/3GC |
R8C/3JC |
R8C/32D |
R8C/33D |
R8C/35D |
R8C/3GD |
R8C/32M |
R8C/33M |
R8C/34M |
R8C/35M |
R8C/36M |
R8C/38M |
R8C/3GM |
R8C/3JM |
R8C/33T |
R8C/3JT |
R8C/3NT |
R8C/36T-A |
R8C/38T-A |
R8C/3MK |
R8C/34K |
R8C/3MU |
R8C/34U |
R8C/3MQ |
R8C/L35C |
R8C/L36C |
R8C/L38C |
R8C/L3AC |
R8C/L35M |
R8C/L36M |
R8C/L38M |
R8C/L3AM |
R8C/LA3A |
R8C/LA5A |
R8C/LA6A |
R8C/LA8A |
R8C/Mx |