Is there disparity in MCU current consumption among 2 methods for pins?
Latest Updated:01/09/2009
Question:
(I/O Port, Electrical Characteristics) Is there a difference in MCU current consumption between the following two termination methods for unused pins in STOP mode:"Set to output mode and leave them open" and "Set to input mode and connect to VCC/VSS through resistor"? [2009/01/09]
Answer:
No, there is no difference in current consumption between the two methods. (#107248)
Suitable Products
3803H |
3803L |
3823 |
3850A |
3858 |
38D2 |
38D5 |
7544 |
7545 |
7546 |
7547 |
7548 |
7549 |