Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is there anything I need when switching from Flash to Mask version?

Latest Updated:01/18/2008

Question:

Is there anything I need to be careful of when switching from Flash version to Mask version?

Answer:

Make sure that the resonator matches in Mask. Also, if necessary, perform noise, current consumption and I/O characteristic evaluations. If you have installed software to access the Flash version-specific register, that portion needs to be deleted. The FWE terminal does not function in Mask version. Please refer to individual hardware manuals for FWE terminal disposal.
Suitable Products
H8S/2649
H8S/2648, 2646
H8S/2643
H8S/2630, 2639, 2638, 2636, 2635
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2378, 2378R
H8S/2368
H8S/2398, 2357
H8S/2345
H8S/2339
H8S/2329
H8S/2319
H8S/2282, 2280
H8S/2268, 2264
H8S/2258, 2239, 2238, 2237, 2227
H8S/2215
H8S/2214
H8S/2218, 2212
H8S/2148, 2144
H8S/2138, 2134
H8S/2128, 2124