Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is there any product which watchdog timer is on the state of power-on?

Latest Updated:03/26/2009

Question:

Is there any product in which watchdog timer is on from the state of power-on?

Answer:

Yes, there are.
Suitable Products
H8/300H Tiny
H8/36109
H8/36077, H8/36079
H8/36049
H8/36912, H8/36902