Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is there a method prevents external device for reading on chip flash?

Latest Updated:03/08/2012

Question:

Is there any method for preventing an external device (other than the CPU) from reading the on-chip Flash?

Answer:

There are two ways to read the on-chip Flash, and there are corresponding functions that protect these accesses. They are as follows:

  • Reading with a parallel programmer
    The ROM code protect function is provided for disabling this type of accesss.
    Setting the ROM code protect control register located in the on-chip Flash disables a parallel programmer from reading or writing the on-chip Flash.
  • Reading with a serial programmer
    The ID code check function is provided for disabling this type of access.
    Once you enable this function (setting an ID code in the on-chip Flash), the MCU will refuse to respond to the serial programmer until the proper ID code is input.

Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A