Skip to main content
Renesas Electronics Europe - Knowledgebase

Is there a if I use 83°C on the product with a maximum of only 80°C?

Latest Updated:08/01/2007


The absolute maximum rating of the operating ambient temperature is 80°C, but I want to use the product at 83°C. Are there any problems?


Yes, there is a problem. The absolute maximum rating must not be exceeded at any time.
Products whose absolute maximum ratings have been exceeded may have suffered the damage even if they seem to be operating normally.

If an absolute maximum rating has been exceeded even slightly, stop using the product and replace it with a new one.

Suitable Products