Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is there a function equal to the one-shot generating mode of 7540 Group?

Latest Updated:09/29/2006

Question:

(Timer, Migration)   In the 7542, 7546 & 7547 Groups, is there a function equivalent to the programmable one-shot generating mode or programmable wait one-shot generating mode of the 7540 Group? [2006/09/29]

Answer:

In the 7542, 7546 & 7547 Groups, there is no mode with exactly the same function as these modes of the 7540 Group timer Z. However, waveform generation by timer A or timer B (output compare function ) can be used to generate a one-shot pulse. (Note that a trigger from the external INT pin cannot be used). (#104957)
Suitable Products
7546
7547