Skip to main content
Renesas Electronics Europe - Knowledgebase

Is the value of TCWE held 0 when it is written in the status of TCSRWD?

Latest Updated:03/18/2009


When using the watchdog timer on the Tiny series when 1 is written to the timer counter W writing enable (TCWE) bit of the timer control /status register (TCSRWD) is the value 1 held until the next 0 is written ?


Yes 1 is held until the next 0 is written.
Suitable Products
H8/300H Tiny