Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is the internal ROM accessed with no-wait in the memory expansion mode?

Latest Updated:03/15/2012

Question:

Is the internal ROM accessed with no-wait under the following register conditions in the memory expansion mode?:
- PM17 bit of the PM1 Register is "0" (no-wait)
- CS0 bit of the CSR Register is "1" (chip select output enabled) and CS0W bit is "0" (with wait)

Answer:

Since PM17 bit is set to "0", the internal ROM area is accessed with no-wait. CS0W bit sets with or no-wait for the /CS0 area.
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/30P