Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is programming of internal memory of uPD78F0058 possible by software?

Latest Updated:12/01/2011

Question:

Is programming of the internal flash memory of the uPD78F0058 possible by software?

Answer:

Unfortunately, flash reprogramming using the user's own program is not supported.
For firmware reprogramming, connect the programmer (Flashpro) via a serial interface externally and perform reprogramming from the programmer.
Suitable Products