Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is it possible to generate an interrupt when M16C/6C receives IN token?

Latest Updated:02/09/2009

Question:

When the M16C/6C receives an IN token from the host, I want an interrupt to be generated if there is no valid transmit data in the endpoint transmit FIFO buffer (the data transmit buffer). Is it possible to generate an interrupt?

Answer:

Yes, it is possible.
In the M16C/6C, you can generate an interrupt if there is no valid data in the endpoint transmit FIFO buffer when an IN token is received from the host.
Suitable Products
M16C/6C