Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is it possible to change transfer direction of the USB endpoints 1 and 2?

Latest Updated:02/09/2009

Question:

Is it possible to change the transfer direction of the USB endpoints 1 and 2?

Answer:

Yes, it is possible.
By changing the value of "the endpoint number used by the host" in the USB endpoint information register (USBEPIR), you can change the transfer direction (IN/OUT) of endpoints 1 and 2 viewed from the host.
Suitable Products
M16C/6C