Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is it possible, output synchronous serial signal from V850 to 16 bits?

Latest Updated:12/01/2011

Question:

Is it possible to output a synchronous serial signal from the V850 in 16 bits?

Answer:

This depends on how much error is allowed.
In a general V850 Series product, this corresponds to repeating 8-bit communications twice.
If the CPU processing is fast enough to perform processing between the 1st byte and the 2nd byte, this method can be used.

The V850/SB1 has a serial communication function to enable synchronous communications up to 16 bits in length.
If the CPU processing is not fast enough, we recommend you use this model.

Suitable Products
V850 Family