Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is it needed to count value set TMR TCORA from post transition mode clock

Latest Updated:01/18/2008

Question:

I'm using a product with a subclock. After directly transistioning between high-speed mode and subactive mode, is it necessary to rerequest the count value set in TMR TCORA, TCORB from the post-transistion operation mode clock? (using TMR as timer interrupt)

Answer:

Yes. Since the post-transistion operation mode clock uses TMR, rerequest is necessary.
Suitable Products
H8S/2282, 2280
H8S/2268, 2264
H8S/2258, 2239, 2238, 2237, 2227
H8S/2218, 2212
H8S/2189R
H8S/2168
H8S/2148, 2144
H8S/2140B
H8S/2138, 2134
H8S/2128, 2124
H8S/2114R
H8S/2111B
H8S/2110B