Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is input or output of TxDi and RxDi pins determined by the setting of I/O?

Latest Updated:09/22/2010

Question:

Is input or output of the TxDi and RxDi pins determined automatically according to the setting of the serial I/O mode select bit?

Answer:

Input or output is not determined automatically.
The function select register needs to be set along with the TxDi and RxDi pins. In addition, the port direction register needs to be set to "0" (input) for the RxDi pin.
Suitable Products
M32C/95
M32C/80
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80