Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

In the uPD78902x, can pull-up resistors be specified by a mask option?

Latest Updated:12/01/2011

Question:

In the uPD78902x, can pull-up resistors be specified by a mask option?

Answer:

Since all on-chip pull-up resistors for the ports of the uPD78902X are switched by software, no item is specified by mask option.
Suitable Products
UPD78902x