Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to reuse program of M16C/60 Series in M16C/80 or M32C/80 Series MCUs

Latest Updated:03/08/2012

Question:

Is there any easy way to reuse the assembly program of M16C/60 Series in M16C/80 or M32C/80 Series MCUs?

Answer:

AS308 has a command option, "-mode60" to assemble the program developed using AS30.
However, some instructions cannot be replaced even by using this command option.
The warning or error message will be displayed for such irreplaceable instructions, so please change the source programs. Please refer to the user's manual for AS308 for the instructions which cannot be handled or replaced by using AS308 "-mode60" option.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80