Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to properly set binary value to register A?

Latest Updated:01/01/2008

Question:

I set the binary value to register A and performed decimal adjust instruction, but was not able to obtain a correct result.

Answer:

The decimal adjust instruction is not for converting binary values to decimal values. To convert binary values to decimal values, a conversion program must be used.
Suitable Products
78K Family