Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to process the JTRST# pin as described in the hardware manual?

Latest Updated:10/29/2005

Question:

The method for processing the JTRST# pin described in the hardware manual of the microcomputer and the manual shown for the M32100T2-SDI-E are discrepant. How should I process the pin?

Answer:

Please refer to the processing method described in the user's manual of your microcomputer. Note that a low on JTRST# input resets the entire circuit of the SDI. Therefore, when you are not using it, supply a low-level signal to the JTRST# pin.
Suitable Products
32170, 32174
32171
32172, 32173
32176
32180
32182
32185
32186
32192
32195
32196