Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to know products that has power on reset and products that do not?

Latest Updated:03/25/2009

Question:

Is there any difference on reset clear timing between the products which incorporate the power-on reset function and the products which don’t incorporate the function?

Answer:

For the product with built-in power-on reset function, internal reset is cleared, 131,072 cycles after the state of RESN signal is set to high.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902