Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How much voltage is needed to run H8S/21xx F-ZTAT memory devices?

Latest Updated:03/18/2009

Question:

What is the voltage supply required to program the H8S/21xx F-ZTAT memory devices ?

Answer:

The H8S/21xx (and all H8S FLASH devices) are single rail FLASH programming devices. This means that a 5V devices operates at 5V and requires 5V to program the FLASH. Even though a 3V devices may operate at 5V it still has to be programmed at 3V.
Suitable Products
H8S Family
  • Was this article helpful?