Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How much external load can be connected to D/A output without a buffer?

Latest Updated:02/27/2012

Question:

How much external load impedance can be connected to D/A output pins without a buffer?

Answer:

If D/A output acceptable errors are less than 2%, the absolute accuracy of the D/A converter is a maximum of 1%. So, it is necessary to make errors due to impedance load less than 1%. Therefore, it is necessary to have resistance value of the connecting load at 99 or more times of D/A converter output resistance.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/5M
M16C/57
M16C/1N