Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How many interrupt modes are supported on the Tiny series ?

Latest Updated:03/18/2009

Question:

How many interrupt modes are supported on the Tiny series ?

Answer:

The Tiny series has a H8/300H CPU core but does not have an interrupt controller peripheral. The Tiny has the same modes as the H8/300L and therefore masking is done by the I bit only. There is therefore only one interrupt mode.
Suitable Products
H8/300H Tiny